Part Number: TPL5110-Q1 Other Parts Discussed in Thread: BQ32000 , BQ32002 Hi, Support Team
do we have different temperature about timer accuracy ppm? (-40 to 85 deg), (85 to 105 deg),(105 to 125 deg)
if any suggestion, Please advise me.
Thanks,
Best regards…
Part Number: TPL5110-Q1 Other Parts Discussed in Thread: TPL5110 Hello, We are using the timer TPL5110 as power management for our device, it works but we faced a problem when we used a cable of 30cm or So, to connect the battery, The voltage is still 3…
Part Number: TPL5110-Q1 Hi Team,
Customer have a few question for TPL5110-Q1
1. If only timing wake-up feature is used, Are they supposed to pull down corresponding voltage on DELAY/M_DRV PIN pin?
2. In the early stage of design, customer wanted to use…
Part Number: TPL5110-Q1 Other Parts Discussed in Thread: TPL5110 Hi team,
Equation of the Tadc is different between TPL5110 and TPL5110-Q1.
Which is the correct equation?
I would like to select time interval = 2.6s.
Tadc from equation (3) in TPL5110 …
Part Number: TPL5110-Q1 Other Parts Discussed in Thread: TPL5110 Hi,
I am using the TPL5110 in the timer mode as a periodic sleep/wake/done with a microcontroller and I noticed that the boards works fine but after testing the boards for a long time like…
Part Number: TPL5110-Q1 Hi Team,
Could you possible help to check if customer use manual mosfet power on applied to the DELAY/MD_DRV pin, And during the M_DRV is high and if there has Done signal input as below picture shows, then, when would the TIP…
Part Number: TPL5110-Q1 Other Parts Discussed in Thread: TPL5110 , TPL5110EVM Dear
Our company refers to "TPL5110EVM User's Guide" and TPL5110 manual application circuit design One shot mode circuit is as follows:
The test found the following…
Part Number: TPL5110-Q1 one shot mode::
1. Is the programmed time interval still selected as shown in 8.5.3? Or a fixed value?
2. In this mode, if the DELAY/M_DRV pin is connected to the power supply through the closed switch during the power-on period…
Part Number: TPL5110-Q1 Hi Team,
I am considering to use a TPL5110-Q1 for power saving, by enabling the main 5 V supply through a pMOS around every second (tIP–50 ms).
I would connect the DONE pin to ground, and the DRV pin to a nMOS that switches…
Part Number: TPL5110-Q1 Hi all,
I got a question of TPL5110-Q1 how to set the time interval of mid value between two values in the lookup table, e.g. 130ms. I don't think this is feasible but can you tell me if this is feasible using this device?
…