Part Number: TPS38-Q1 Other Parts Discussed in Thread: TPS36-Q1 , TPS35-Q1
Can the watch dog be proactive disabled with Pin Configuration Option A? (means WDI output low level all the time)
Part Number: TPS3850 Other Parts Discussed in Thread: TPS35-Q1
Hello team,
Is there similar one or p2p device with below Rohm items? thanks.
BD820F5UEFJ-CE2
BD37B28FVM-CTR
BD87B28G-CTR
BD87B28FVM-CTR
Part Number: TPS3435-Q1 Other Parts Discussed in Thread: TPS36 , TPS3436 , TPS35 , TPS3435 Tool/software: Hi TI,
I'm working on a project using the TPS3435AFACADDFRQ1.
Now we use this watchdog timer as a failsafe circuit to make sure the system is safe…
Add-On:
The TPS35-Q1 has separate /RESET and /WDO outputs and a orderable(?) option with latched outputs. The behavior after entering the latched state is described on page 24: /RESET remains high, /WDO remains low. (The described AND for both signals…
Part Number: TPS3431 Other Parts Discussed in Thread: TPS35-Q1 , TPS3435 , TPS3851 , Hi team,
Could you confirm whether the WDI pin can support 16MHz?
Are there any devices whose WDI pin can support 16MHz? Do you think devices below can support it?
TPS35…
Hi Grady,
For monitoring device operation we have two options. Timeout Watchdog or Window Watchdog.
A watchdog device, in general, requires a pulse from a controller (i.e CPU, MCU, SoC, etc) within a specific time, if a pulse is not received by the watchdog…
HI Dave,
We are currently in the process of releasing a new watchdog part, TPS35-Q1. This device is a supervisor + Watchdog with programmable watchdog timeout delay. The variant available for sampling at the moment has a voltage threshold of 2.9V.
https…
Part Number: TPS3850-Q1 Other Parts Discussed in Thread: TPS3703-Q1 , , TPS35-Q1 , TPS36-Q1 , TPS3850 , TPS35 , TPS36 Hi, Team:
Can you help to check if can power Vcore before VIO voltage?
The application is customer want to power the VIO to get lower Iq while…
Hi Jeff,
Thank you for your question. The TPS3824 is the pin-to-pin replacement for this part.
https://www.ti.com/product/TPS3824
But since this is an older part I would like to recommend our TPS35-Q1
https://www.ti.com/product/TPS35-Q1
Jesse
Part Number: TPS3850-Q1 Other Parts Discussed in Thread: TPS3850 , , TPS35 , TPS36 Hi team,
I would like to know if I can disable lower boundary of watchdog timer in TPS3850 to use it as simple Time out type watchdog.
Is that possible?
regards,