The inhibit pin disables the VCO, but the VCO output might stop in either the high or the low state. (I do not know what you're doing with the phase comparator; please show a schematic.)
As far as I can see, the CD4046B itself cannot put its output…
Hi Ben,
The TS5A22362 only has a bandwidth of around 18MHz so it will not be able to pass a 100MHz clock signal. For all of those specifications, you would need to look into something with dual supplies as we do not have a part that can do that higher…
Other Parts Discussed in Thread: TS12A12511 Looking to use a switch with the features of the TS12A12511 in an audio circuit where the power supplies are +/-15V. This is beyond the rating of the TS12A12511. Do you have a device currently available or about…
Other Parts Discussed in Thread: TS12A12511 I am using a pair of TS12A12511 switches in an analog signal line switching application. An ADC directly controls the switches. I am using +/- 2.5V signal voltage levels. Unfortunately the converter does not…
Other Parts Discussed in Thread: TS12A12511 Howdy folks,
Quick question on the TS12A12511. I'm inputing 2 analog signals into the normally closed the normally open pins and would like to switch between them using a TTL signal. Should the GND pin on…
Part Number: TMUX1136 Other Parts Discussed in Thread: TS12A12511 , , TS5A22362 So, what is the actual lower end of the analog signal range? 0.00mV? Some other value?
I could save PARTS if the limit extended below 0.00mV, even a little bit.
Thanks in advance…
Other Parts Discussed in Thread: TS12A12511 Howdy,
Are there any models out there for any of the analog switches ( http://www.ti.com/lit/sg/slyb125d/slyb125d.pdf )? Specifically the TS12A12511.
TINA TI is a fantastic tool!
Thanks,
Austin
Hi Denny,
The closest pin-to-pin device we have for this part would be the TS12A12511 in the DRJ package. However, there is one difference in that the TS12A12511 has a VSS on what the NL5S4257B-D has as a no-connect (NC) pin, so they would need to be able…
Part Number: TMUX6112 Other Parts Discussed in Thread: TS12A12511 Hi Team,
As titled, customer wants a switch that can short the channel (D to S) when VDD/VSS is not applied (0V).
If no, further question is if there is existing device in TI that does so…