Part Number: TUSB1210-Q1 Hi Team,
How much current will the REFCLK pin consume when it is active? I see that there is a specification in the datasheet for 3uA when in HI-Z, but there is no spec for when it is active.
Any insight you can provide would…
Part Number: TUSB1210-Q1 Hi Team,
If OTG is not going to be used and therefore the ID pin will not be used, what should be done with the ID pin?
Thanks,
Jared
Part Number: TUSB1210-Q1 Hi Team,
In the pin functions, should the N/C pins include pin 25? I am assuming "yes" and that putting pin 24 twice was a mistake, but please confirm.
Thank you,
Jared
Part Number: TUSB1210-Q1 Other Parts Discussed in Thread: TUSB1210 , Hello,
I saw on this thread ( https://e2e.ti.com/support/interface/usb/f/1008/t/522352 ) that the TUSB1210 timing issue with Zynq-7000 was solved.
I need to use the automotive grade version…
Part Number: TUSB1210-Q1 Hi Team,
Could you please help to check if we have USB PHY to SPI transceiver? Customer wants to add an USB interface to their system, but their MCU just have SPI interface..
Other Parts Discussed in Thread: TUSB1210-Q1 Hi,
My customer would like to confirm the power sequencing of TUSB1210-Q1.
Is there any specification for the power supply start-up/down timing?
Is it following only?
Though I found following thread on the…
Part Number: TUSB1210 Other Parts Discussed in Thread: TUSB8041-Q1 I have a TUSB1210BRHBTQ1 USB2.0 phy connected to an embedded linux device and downstream of the USB phy I have a TUSB8041IPAPRQ1 2.0/3.0 hub connected. I'm trying to use the USB phy purely…
Part Number: TUSB1210 Hello,
I'd like to know if the output capacitance of TUSB1210-Q1 really needs to be > 120uF in Host Mode. Why is it that high and under what circumstances can it be lowered?
In Device Mode it is 4.7uF - can that capacitance…