Part Number: TVP5150AM1 Other Parts Discussed in Thread: TVP5150 Hi,
i built my own PCB with the TVP5150 to run this with an STM32F407. The comunication over I2C is ok and i can write/read all registers. I configuered a default setup for the TVP5150 and…
Part Number: TVP5151 Other Parts Discussed in Thread: TVP5150 Hi Team,
Could TVP5151 or TVP5150 use in CVBS to DVP?
What display resolution screen does TVP5151 support and how much refresh rate can it achieve?
Part Number: AM5728 Other Parts Discussed in Thread: TVP5150AM1 , TMDSEVM572X , TVP5150 , BEAGLEBOARD-X15 , DRA752 , TMP102 , PMP , TVP7002
hello
I want to add device tree for TVP5150AM1 in AM5728 EVM linux SDK and use it instead od Camera module. my SDK version…
Part Number: TVP5150 Hello I have a AHD camera with the resolution 720p output, I want to decoder the AHD output to 8-Bit 4:2:2, so can the tvp5150 be access to this task, I know it can support the PAL input, but I am not very sure it can also support…
Part Number: TVP5150 Other Parts Discussed in Thread: TVP5151 Hi,
We have the tvp5151 chip as a decoder connected to the analog video input. We need to support both PAL and NTSC standard videos . To detect the hot plug events we used the the Register1…
Part Number: TVP5150 Hi Everyone
I am working on a project which is about capture video.
When the system starts(Video input enable) everything is good. The video seems to start at top of the monitor. Everything is flawlessly but the system starts(video…
Part Number: AM5728 Other Parts Discussed in Thread: TMDSEVM572X , TVP5150
hello
I have designed two video receiver boards for interfacing BT.656 or BT.1120 pixel bus with TMDSEVM572x board.
in one board I have used the chip TVP5150AM for converting PAL…
Part Number: AM5728 Other Parts Discussed in Thread: TVP5150AM1 , TMDSEVM572X Hello
I have a problem with capturing interlaced video from TVP5150AM1 in TMDSEVM572x and deinterlacing it.
I have used this commands :
root@am57xx-evm:~# gst-launch-1.0 -e v4l2src…
Part Number: TVP5150
Hi,
how can I set the routing of the TVP5150 from userspace? Is there a way to do this over v4l2-ctl?
I saw in the kernel driver that there is an initalisation for an v4l2_i2c_subdev and there is a function selmux, but how can I…