Part Number: AFE58JD48EVM Other Parts Discussed in Thread: TX517 , TX7316EVM , , TSW14J50EVM , TX7516EVM , AFE58JD28EVM Tool/software: Dear TI Team,
I am currently working on developing an ultrasound imaging system using TI’s EVMs. Based on information…
Part Number: TX517EVM Other Parts Discussed in Thread: TX75E16 , TX7516 , TX517 I went through this thread , can you let me know what power supply you used for powering up P1 header in TX517EVM board
Part Number: TX517EVM Other Parts Discussed in Thread: TX517 , Hi,
I measured the OUTA and OUTB waveform, and got a different result from the datasheet.
What could be causing part of the waveforms to differ from the datasheet?
HV0:+1.9V,LV0:-1…
Part Number: TX517EVM Other Parts Discussed in Thread: TX517 , Hi,
I measured OUTA and OUTB waveform according to advice, but could not get the waveform as shown in the datasheet.
connection setting:HV0:+1.9V,LV0:-1.9V,HV1:+15.0V,LV1:-5.2V,HV2:+8…
Kiyong,
Thanks for looking at the TX517! we are not be able to share the FPGA code due to liability concerns.
maybe we can discuss this request off line. you can send an email and customer contact info to mysecuresoftware_medical@list.ti.com
we…
For those of you who might need the answer to this question. These VAA, LV0, and HV0 Pins are all connected to U20 (TX517). If you read the manual of this chip (TX517), you could see the minimum required current for each pin. It's on page 9 of www.ti…
Hi Olu,
Are you sure that there is no minimum frequency requirement? Here is the recommended operation conditions for the TX517 according to the user manual ( www.ti.com/.../tx517.pdf):
The INNxx, INPxx input sample rate has a minimum value of 1…
Hello Xiaochen,
Thanks for the patient reply.
Is there any alternative to TX517 that could be used for imaging purpose ?
Since I'm looking for an end-end solution, I don't prefer using any ready-made imaging platform. Instead I prefer to do necessary…
Hi Kai,
so what i am trying to do is what the TX517 is for, an ultrasound trasmitter.
But i am not using CPLD or FPGA jus a MCU. So i want to make a sine wave pulse with an opamp.
Do you know a TI opamp that can handle 150mA output current, can be…
Other Parts Discussed in Thread: TX517 In a previous post it was confirmed that the voltages HV1, LV1, HV0, LV0, HV2, LV2 + VDD, VEE, VCM must be supplied externally to the evaluation kit. In addition the datasheet states - the max power supply slew rate…