Part Number: DP83TG720S-Q1 Other Parts Discussed in Thread: TXV0106 Tool/software: Hi Teams:
When the PHY chip is powered down, the RXD0~RXD4 and RX_CTRL pins output a short 125MHz square wave signal. We have tested and found that the VDD3.3V, VDD1.0V…
Part Number: TXV0106 Other Parts Discussed in Thread: TXV0108-Q1
Hello Team,
shouldn't Vcca and Vccb be switched for the lower part as this is a unidirectional level shifter?
Also Vout(min) should be corrected to 1.14V in the search parameters, right…
Part Number: SN74AXC4T245 Other Parts Discussed in Thread: TXV0108-Q1 , TXV0106-Q1 Hi Team,
We are using the SN74AXC4T245PWR IC for level translation. In the datasheet, it is given that the data rate supported whea.n translating from 1.8V to 3.3V is up…
Part Number: SN74LVC2T45 Other Parts Discussed in Thread: TXV0106-Q1 Team,
Can we consider that the propagation delays of falling transitions are the same between both component lanes (1 and 2)?
Or is there a significant gap?
Same question for the propagation…
Hi All,
Please see the new TXV level-shifter family (TXV0106-Q1 / TXV0108-Q1) supporting high-bandwidth timing-margin sensitive interfaces such as RGMII.
For more information, see Enabling high performance interface translation | Video | TI.com , thanks…
Part Number: SN74AXC8T245 Other Parts Discussed in Thread: DAC900 , , TXV0108-Q1 , TXV0106-Q1 Hi team,
When I use multiple SN74AXC8T245s , what is the skew between the devices?
The system has 11 bits of clock and data, so I am concerning.
(I understood from…
Hi Jeff,
We actually released a new translator family specific to tight timing budget applications such as RGMII.
Please help see TXV0106-Q1 and TXV0108-Q1, thanks.
Best Regards,
Michael.
FAQ: Logic and Voltage Translation > Voltage Translators >> Current FAQ
Here are the voltage level translation device recommendations for various industry standard interfaces:
Interface
Recommended Device
3.6V Maximum
5.5V Maximum
FET R…