Part Number: MSP430F5132 Other Parts Discussed in Thread: UCC27517 Tool/software: In Tida 00121 design,
U2 -UCC27517DBV should be grounded with Power ground, but in schematic it is not like this what is your suggestion think it should be.
Part Number: ISO7740 Other Parts Discussed in Thread: UCC27517 Tool/software: Hello,
I wanted to know current source capability of individual channel of digital isolator part ISO7740. Below plot is from ISO7740 datasheet, is this plot is for individual…
Part Number: UCC27518 Other Parts Discussed in Thread: UCC27519 , UCC27517 , Tool/software: Can this be fixed?
The unencrypted model is still broken...
Specifically this line (at least) is incorrect
** X_U1_U4 U1_UVLO U1_EN_OK U1_INM_OK DRV AND3…
Part Number: SN74ACT244 Other Parts Discussed in Thread: UCC27517 Tool/software: I am trying to connect several output pins of SN74ACT244 to obtain a drive capacity of more than 100mA. I will be driving a 50Ω termination. I am thinking of attaching a…
Part Number: UCC28180 Other Parts Discussed in Thread: UCC27517 Tool/software: Dear Experts,
The following is the circuit schematic of our 1.5KW PFC. Please help review if the design is reasonable. Thank you
Design requirements: Power supply voltage…
Part Number: SN74HCS126 Other Parts Discussed in Thread: SN74AHCT1G125 , UCC27517 , SN74AHCT125 Tool/software: Dear TI team,
I am going to use IC- SN74HCS126 to buffer uC 3.3V PWM (Freq- 50 kHz to 500 kHz) to 5V logic level.
I need to confirm below…
Part Number: TCA6408A Other Parts Discussed in Thread: CSD17571Q2 , UCC27517 Tool/software: Maybe it's just late and I'm tired, but I just want to check myself here. Can you use the I/O pins of the TC6408A to directly drive MOSFETs (specifically the CSD17571Q2…
Part Number: LMH7324 Other Parts Discussed in Thread: TLV1872 , THS4041 , , TLV3601 , UCC27517 Tool/software: Hello,
TLV1872 (65ns, 40V, dual) is too slow compared with ISL55142IVZ.
Is it possible to replace this function with a fast comparator with…
Part Number: SN74LV14A Other Parts Discussed in Thread: UCC27517 Iok is specified to be up to -50 mA.
Does this mean that there is no clamp diode with the + side?
I want to drive the gate of the FET, is 7V still acceptable?
I think that Vcc + 0…
Part Number: TIDA-050063 Other Parts Discussed in Thread: TPSI3052-Q1 , UCC27517 Tool/software: Hi team,
Because of the limited power transfer capability of the TPSI3052-Q1 it is hard to find a suitable Inductor. I would like to have a smaller peak…