Part Number: TCAN1145-Q1 Hello Expert,
My customer is designing circuit with TCAN1145-Q1 for CAN FD bus. From the view point of design diversion, they are considering to use it for Classic CAN bus as well.
For this diversion, is there any specific concern…
Part Number: TPS61240-Q1 There are 2 package schematics for SON in the datasheet. DRV0006A and DRV0006D. Why 2? And which package is for which product?
There is obvious difference between them.
Please make it clear which one of the packages is for each…
Part Number: UCC2813-5-Q1 I took the help of WEBENCH POWER DESIGNER for design of my Fly back converter of 56 w. My design no. 146.My user Id is info@aeshyd.com. when I click on the transformer, its showing popup with transformer information as CUSTOM…
Part Number: DS90UB935-Q1 hi team,
Below spec is very confusion as the max is lower than typical while min is higher than typical, can you help clarify?
Regards,
Dongbao
Part Number: AM62A3-Q1 Hi,
I am trying to implement 2 ethernets using the AM62A3-Q1, I have mapped the RGMII signals to RGMII1 and RGMII2 in CPSW3G0 domain. But I see there is only one set of MDIO and MDC in the processor while generating the .dtsi file…
Part Number: DS90UB954-Q1 Other Parts Discussed in Thread: DS90UB953-Q1 ,
We are facing an issue with streaming(Streaming is not happening). I will include the register dump of Deserializer(DS90UB954-q1) and serializer(DS90UB953-q1) here. I am trying to…
Hello Amy,
To which 960 RX port is the 953 connected?
Are you switching from Mode #2 to #3 or the opposite?
Are you making any register changes on the 953 when you are making this switch? You need to make some changes in reg 0x05
can you provide register…
Part Number: UCC2813-5-Q1 I took the help of WEBENCH POWER DESIGNER for design of my Fly back converter of 56 w. My design no. 146.My user Id is info@aeshyd.com.
Another clarification required. you said NS1 is secondary and NS2 is auxillary. But the winding…
Part Number: PCM1820-Q1 Other Parts Discussed in Thread: PCM1820 , ADS7057 , THS4561 , TI support,
For the PCM1820 ADC output, the code range (2's compliment) for the negative voltage range does it include the negative values?
In the application note…