Part Number: UCC2813-5-Q1 I took the help of WEBENCH POWER DESIGNER for design of my Fly back converter of 56 w. My design no. 146.My user Id is info@aeshyd.com.
Another clarification required. you said NS1 is secondary and NS2 is auxillary. But the winding…
Part Number: DS90UB936-Q1 As I understand from the Pin description table, we need to pull VDD_SEL = LOW to have the 1V1 rail be internally generated.
However, the connection of VDD_SEL to 1.8V in Figure 8-4 of the datasheet, appears to contradict this…
Part Number: DP83TG720S-Q1
Attached are the latest drivers tested on Kernel 5.10: GitHub - TexasInstruments/ti-ethernet-software: Repository for Ethernet PHY drivers for Linux and RTOS.
The DP83TC812 driver can be used for the DP83TC813 and DP83TC814…
Part Number: DRV3901-Q1 Hello,
I am new to pyro-fuses but was wondering if you could check if DRV3901-Q1 is able to drive a PSS-4, battery disconnect switch.
Datasheet: PSS-4_DataSheet_06-2019_Rev015 (autoliv.com)
Hi Tony,
You are right.
Tony Han said: So, When I test buck mode, Vout = 14.5V ==> Max Power output is 2.6kW
I believe it is possible to have 3 EVMs in parallel.
Follow Figure 8-23. Six Phases 120° Interleaving Configuration in the datasheet and …
Part Number: OPT3001-Q1 Other Parts Discussed in Thread: OPT4001-Q1 Hi Team,
I would like to check if our OPT3001-Q1 and OPT4001-Q1 can meet the spec or not. smoke print spec 14%+-4% in 550nm
Regards,
Roy
Part Number: ADS1261-Q1 Hello,
I am looking for 3 wire and 4 wire RTD design using ADS1261-Q1. The datasheet provides only information on 3 wire circuit. Kindly guide us for 4 wire RTD design.
Part Number: DS90UB964-Q1 Hi Team,
My customers are using DS90UB964 to deserialized signal from 4 cameras and 4 Serializer with DS90UB933, but the cameras' resolution are different, first three signals are 1280x960x30fps and last one is 1280x720x30fps…
Part Number: LM5185-Q1 Other Parts Discussed in Thread: LM5185 Hello, please consult our input voltage 4-40V, we want to output voltage 12V, current 1A, can we use the LM5185-Q1 chip to achieve? thank you.