Part Number: UCC2813-5-Q1 I took the help of WEBENCH POWER DESIGNER for design of my Fly back converter of 56 w. My design no. 146.My user Id is info@aeshyd.com. when I click on the transformer, its showing popup with transformer information as CUSTOM…
Part Number: UCC2813-5-Q1 I took the help of WEBENCH POWER DESIGNER for design of my Fly back converter of 56 w. My design no. 146.My user Id is info@aeshyd.com.
Another clarification required. you said NS1 is secondary and NS2 is auxillary. But the winding…
Part Number: TPS25772-Q1 Other Parts Discussed in Thread: TPS55288 , Hello,
I am designing a 4 port USB-C PD system for a vehicle, I am using TPS25772 + TPS55288, and was not able to understand the proper method for firmware updating. I see it can be done…
Part Number: TPS6594-Q1 GPIO 4 pin is configured as an output. When pulled up by external VCCA, the voltage of GPIO 4 cannot be raised to 3.3V, and it remains at only 0.74V. I would like to inquire about the cause of this issue.
Part Number: DS90UB936-Q1 As I understand from the Pin description table, we need to pull VDD_SEL = LOW to have the 1V1 rail be internally generated.
However, the connection of VDD_SEL to 1.8V in Figure 8-4 of the datasheet, appears to contradict this…
Part Number: DRV3901-Q1 Hello,
I am new to pyro-fuses but was wondering if you could check if DRV3901-Q1 is able to drive a PSS-4, battery disconnect switch.
Datasheet: PSS-4_DataSheet_06-2019_Rev015 (autoliv.com)
Part Number: OPT3001-Q1 Other Parts Discussed in Thread: OPT4001-Q1 Hi Team,
I would like to check if our OPT3001-Q1 and OPT4001-Q1 can meet the spec or not. smoke print spec 14%+-4% in 550nm
Regards,
Roy
Hi Tony,
You are right.
Tony Han said: So, When I test buck mode, Vout = 14.5V ==> Max Power output is 2.6kW
I believe it is possible to have 3 EVMs in parallel.
Follow Figure 8-23. Six Phases 120° Interleaving Configuration in the datasheet and …
Part Number: DP83TG720S-Q1
Attached are the latest drivers tested on Kernel 5.10: GitHub - TexasInstruments/ti-ethernet-software: Repository for Ethernet PHY drivers for Linux and RTOS.
The DP83TC812 driver can be used for the DP83TC813 and DP83TC814…