Part Number: TDA4VH-Q1 Other Parts Discussed in Thread: SYSCONFIG Tool/software: Team, I was looking at the below post: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1552878/tda4vh-q1-how-should-i-troubleshoot-a-link-up-failure…
Part Number: TICSPRO-SW Other Parts Discussed in Thread: LMX2592EVM , USB2ANY Tool/software: Hi.
I am trying to use the LMX2592EVM with the TICS-PRO via USB2ANY. The problem description is as follows:
1) When I connect the USB2ANY to the pc, it shows…
Part Number: MSPM0G1507 Tool/software: I am developing a flash programmer for MSPM0 that runs on a Teradyne In-circuit tester that runs through the SWD.
I have successfully developed this Flash Programmer for the MSPM0G1507.
The data I program to…
Hang,
This is strange. Are you using same method to load the code on both the boards and also version of SW is same. Also can you disable "Run to main" option and then re-check the content ? If you are loading the code in RAM only and not getting the…
Hello Stuart,
Thanks for the extra information. What I don't fully understand is what that meaning of the SW image being developed by a third party (is it correct to assume it is not TI's SDK?), are you making reference to the boot-loader here (MCUBoot…
Andrea,
Below is what I found in the readme file that came with the prg2xxx programming SW, it does not appear there is a verify only option with this utility.
PRG2XX -[options] c2xxprog.out flashcode.out
Option Description.
-h Help, Lists the options…
Subramanya
Can you please try the following sequence,
Right click on the "TUSB9260 Boot Loader"
Choose to "Update Driver"
Choose to "Browse my computer for drivers"
Choose to "Let me pick from a list of available drivers on my computer". …
Hello,
Yes it is possible to burn flashes form noboot on the EVM with TRACE32/Lauterbach. You will need to look to the specific SW you want to burn for the layouts. There is an application note here which can help: https://www.ti.com/lit/an/spracy5…
Hi Dung,
thanks for running this test. Can we try to summarize all potentially relevant differences of your design vs. the experiment you run on SK-AM62 from a HW and SW perspective? Such as...
TI SK-AM62B
Your Design
OSPI Flash Device…
Part Number: AM2434 Dear Champs,
Is it possible to overlay boot-loader SW by application SW code section?
If so, could you please share some example cmd file and idea how it can be implemented?
Thanks and Best Regards,
SI.