Part Number: AMC1301EVM Other Parts Discussed in Thread: AMC1301 Hi I am using the AMC1301 for high voltage side voltage measurement.
Even though i have scaled down my voltage levels to 3V level from 400V through resistor divider.
Do i need input buffer…
Part Number: AMC1301EVM Other Parts Discussed in Thread: AMC1301 , AMC1200 , Hi team My customer wants to change from AMC1200 to AMC1301 to improve offset voltage. I think analog input of AMC1301EVM do not need the filter (made by resistance and capacitance…
Part Number: DRV421EVM Other Parts Discussed in Thread: DRV421 , INA253EVM , , DRV425 , INA253 , AMC1300 , AMC1200 , DRV5053 , AMC1301EVM , DRV425EVM Hello,
We have LMG3411EVM-18 daughter boards and we want to use them in closed current loop mode. We found 2 EVMs…
Dear Sam,
thank you for your interest in TIDA-00915 and current/voltage sensing. The TIDA-00915 GaN inverter is rated for 200-400V DC-link voltage and the LMG3411 are isolated from the C2000 controlCARD. An inline shunt requires an isolated amplifier…
Part Number: AMC1301-Q1 Other Parts Discussed in Thread: SN6501 , AMC1301EVM , AMC1301 Hi All,
Datasheet recommends 5V for VDD1 though the range is from 3 to 5.5V
I would like to know whether VDD1 and 2 can be given 3.3V from the same source or not. Appreciate…
Hi Jean!
Welcome to our e2e forum! You are correct in that the AMC1301EVM does not tie VINN directly to GND1, since we don't know the exact configuration each customer would like to use with the evaluation module, we left the hardware flexible. The…
Part Number: AMC1301 Hi support team,
My customer had a urgent issue while using AMC1301 for HV current sensing. They followed AMC1301EVM circuit for the input stage and found when they placed a 1uF cap for the differential mode filter cap, there will…