Part Number: AMC1311-Q1 Other Parts Discussed in Thread: AMC1311 , Hello Team,
i have a query, i need the Failure mode distribution of AMC1311 along with the FIT rate information. I couldn't find it .
Part Number: AMC1311-Q1 Other Parts Discussed in Thread: AMC1311
This is the picture of our voltage sensor model using AMC1311 for the closed loop control of boost/buck converter.
The simulation is working fine but when it comes to the physical hardware…
Part Number: AMC1311 Hi Team,
What's the spec of working voltage meaning, how can I understand it and explain to customer? In the system level. Thanks in advance.
BRs,
Francis
Part Number: AMC1311 Hi,
The datasheet of AMC1311 doesn't specify a maximum DC isolation voltage for 60 sec, is there a value for that?
I assume it's 7071 V like the other ones (in the attached picture) because they all have Vrms = 5000 V and they…
Part Number: AMC1311-Q1 Hi Eva,
Per talked, we can follow up below discuss here:
https://e2e.ti.com/support/amplifiers-group/amplifiers-internal/f/amplifiers-internal-forum/1346937/amc1311-q1-failure-at-350v-hv/5132402#5132402
Thank you!
Marc
Hi Frank,
Frank QIN said: Should we consider OUTx as voltage source to do the calculation?
Yes, this should be fine. the OUTx pins can drive 14mA's of current, it can be considered as a voltage source when connected to a high impedance.
Frank QIN said…
Hi Eva,
I have added a 12 pF capacitor in parallel to 1 kOhm sensing resistor. In the following image, you can find the FFT spectrum of the output noise of the current setup. I have noticed, just by the eye, that the low frequency peaks has moved to the…
Part Number: AMC1311 Other Parts Discussed in Thread: AMC3311 Hello everyone,
I'm designing a frequency controller and want to measure rectified DC voltage using an AMC1311. I based my circuit on an application note and would like to confirm if my connections…
Part Number: AMC1311 Other Parts Discussed in Thread: TINA-TI Hi Team,
My customer is using our AMC1311B in their design and are looking for the Simetrix model. Do we possibly have one for this part?
Thanks!
BR,
Alfred Logico