That means Main domain (CPSW9G) signal CLKOUT (pin AA25 / AJ28 /Y29) or WKUP/mcu domain signal MCU_CLK_OUT0 (pin H27) both used the sync TDA4 RMII and PHY RMII REF CLK.
Question:
1. How about the CLKOUT driver strength, does it can driver 3 PHY and route…
Part Number: TPS6521815 Other Parts Discussed in Thread: TPS65218D0 , TPS51206 , TPS65218 , TPS51200 Hello,
Hope you are doing well,
We are using TPS6521815 PMIC for powering Cyclone V GX with DDR3 memory, having few queries with sequencing and configuration…
Part Number: TMS320C6655
Hello,
In our current setup we are booting TMS320C6655 without IBL, we are flashing code into the NOR flash memory(MT25QU128) with help of NOR-Writer utility which perfectly working fine.
ref - https://e2e.ti.com/support/processors…
Hi Vijay,
Yes, you can set the output voltage to be 2.2V, 2.1V or 2.0V by changing the REF resistor using equation 5 in the datasheet (also shown in your screen shot). Iref = 50uA so for each voltage you would need to set the REF resistor to the following…
How are you handling the /LDAC function? It looks like you can drive the output(s) by:
1) Wiggling the /LDAC pin (after writing the code register(s)) [Ref data sheet (Rev 4) p. 12]
2) Using the LDAC command over the SPI [Ref Table 1]
3) Using the Writethrough…
1) Yes, this appears to be the correct setting [per timer_a.h]:
> #define TIMER_A_CLOCKSOURCE_EXTERNAL_TXCLK TASSEL__TACLK
I don't think you need to change anything else (but try it and see).
2) TA1CLK is available on P1.6 (pin 6 on the PT/RHA packages…
Hi Skyler,
Thanks for your feedback here, I would like to double check if we have some ref code use 3-generation C2000(like 280049/25/13)
Thanks
Jenson
If you're using an external (e.g. benchtop) power supply, be sure to connect the MSP-FET using J1 ("VCC TARGET"), not J2 ("VCC TOOL"). [Ref Hardware Tools UG (SLAU278AH) Fig 2-3] If you use J2 you'll have a conflict between the two supplies.…
1) The first 2 bytes you send are interpreted as the EEPROM address to use (high-order byte first) [Ref data sheet (DS21754M) Sec 6.1]. In the code you posted this is 0x0001. You may want to expand to data[2+DATA_SIZE] and explicitly put the address you…
Part Number: TDA4VM-Q1 Hi, Erick
Customer now meet GPU issue. They do pressure test, 30 seconds power on, 10 seconds power off. Issue reproduce about once every 2000 times.
Scenario is power on, issue happen, there is no display in the screen. After 17…