Part Number: DRV2603 Other Parts Discussed in Thread: DRV2624 , DRV2625 Tool/software: Hi All,
I am looking for a suitable driver for CLF-16WX01, can it be driven by DRV2603?
product.minebeamitsumi.com/.../CLF-16WX02.html
Best Regards, Ishiwata
Part Number: LM5158 Dear Team,
Please help confirm about LMf5158 UVLO RUVLOT and RUVLOB value by today.
Our customer would like to have 47DC ON and 36VDC OFF. Thanks a lot.
Many Thanks,
Jimmy
Part Number: TPS548C26 Dear Team,
I have a question need to check with you.
According to Webench suggest schematic, what is the Cnoise is used for?
I saw the Cnoise can be de-pop on other project of our team.
So I’m checking with you about Cnoise…
The new one is incorrect. The first one was almost correct, you just had to swap SRN and SRP. The new one won't work at all as you basically short out the battery by connecting BAT+ to BAT- with the 0.01 Ohm sense resistor.
Hi Jimmy,
In order to generate the same passband frequency response, you can use the same R/C component values as shown above. This will provide you with the same frequency response as I have shown below.
However, as I stated previously, the bandwidth…
Part Number: DRV2603 I have used DRV2603 part in our design to drive https://www.vybronics.com/coin-vibration-motors/lra/v-g0832013d
What if we configure DRV2603 in LRA mode and connect a ERM motor
What if we configure DRV2603 in ERM mode and connect…
Hi Jimmy,
Hope you had a great weekend and thank you for your question.
I noticed that in your calculation for Vout you have the Vnr/ss value as 0.5V*(1+r1/r2) but it should be 0.8 so you will not get your expected Vout with those resistor pairing. The…
Hi Jimmy,
I believe the reason that DRV2603 say that it is Immersion compatible is to let customers know that it is able to reproduce the waveforms from immersion. there also used to be a firmware library that contained the immersion waveforms which was…
Part Number: DRV2603 Dear Team,
If MCU side voltage is 1.9V.
May I know the DRV2603 setting as below is OK?
VDD:3.3V,EN、PWM、LRA/ERM: 1.9V
Many Thanks,
Jimmy
Part Number: DRV2603 Hello team,
My customer has some questions. Would you please advise?
1. Is it necessary to insert a diode to counter the reverse voltage of the motor? The customer do not think that they need it. Is that correct?
2. If a reverse…