Part Number: INA196 Other Parts Discussed in Thread: INA293 , INA281 Hi,
2 or 3 years ago I was working on a design that uses the INA196 part. We struggled quite a bit with the Low Vsense behaviour, which gave us an output voltage, even though the Vsense…
Part Number: INA196 Other Parts Discussed in Thread: INA271-HT Hey team,
I'm looking for a high temperature replacement for INA196, one that can work at 175C.
I'm aware of the INA271-HT, would this be a good replacement or are there more High Temperature…
Part Number: INA196 Other Parts Discussed in Thread: INA190 I have come across several designs that use the INA196 in a 4-20mA receiver, using a 4.99 ohm resistor and an ADC to read in the voltage. We created a circuit that has 5x of these on the board…
Part Number: INA196 Hi team.
I'd like to need a graph of Low Vsense Cases with a voltage of 20mV ~ 150mV.
Can I extend this graph of ideal in the data sheet?
Sincerely.
Kengo.
Part Number: INA196 Other Parts Discussed in Thread: INA126 Hello, I am using an INA196 current shunt for monitoring the signal coming from a dc-dc buck converter (48V to 36V and Io =380mA) which is set up at 430KHz.
I have red in the datasheet that the…
Part Number: INA196 Other Parts Discussed in Thread: LMC6482 Hi
I'm using the INA196 to sense the current of my DC/DC stage. I have to change the output voltage from 0V up to 52V.
I have two issues:
1) Feedback voltage to the current sense resis…
Part Number: INA196 Other Parts Discussed in Thread: TINA-TI , INA193 , INA198 , INA194 , INA195 , INA197 Hello,
I'm using INA196 to measure current flowing through the load as per attached picture. I have wide range of currents, so I use INA196 to measure…
Part Number: INA196 Other Parts Discussed in Thread: LM5069 , , INA303 , INA302 , INA301 I want to know if it is possible to share the shunt of the LM5069 for an inrush current protection with an INA to monitor the used acutal current.
i do not like to use…