Part Number: LM358A
需要先将该运单号取消然后再重新进行预约取件。按照你们以往的操作模式,这次重新下单进行预约取件的账户需要供应商填写他们自己的本地账户,付款方照常填写东莞启益公司的账户,到时系统会给你们发送一份授权邮件确认该笔运费由你们为供应商支付。 不重新预约取件,快递无法发出。
Part Number: LM358A Other Parts Discussed in Thread: LPV802 emma_bode.TSC emma_lpv802.TSC
Hi,
I have built a PIR AFE circuit closely based on this reference design.
The differences are as follows:
- using LM358AMX/NOPB (dual amp in SOIC package)
- reduced…
Part Number: LM358A Other Parts Discussed in Thread: LM358 , LM358B , LM2904B , LM2904BA , LM358BA , Hello,
The data sheet of LM358 family (SLOS068AA) has a functional block diagram in the section 8.2 Functional Block Diagram , but is it applicable to the L…
Part Number: LM358A Hi, all.
I would like to check the value of sink current about LM358A.
Is this the value of sink current under the following conditions?
This is the red frame.
Vid=-1V, Vo=200mV
Best Regards,
Ryusuke
Part Number: LM358A Other Parts Discussed in Thread: LM358 , LM358-N , TLV9002 , LM358LV Hi,
Compared with LM358-N and LM358 D/S,
The output swing specs are a little different
LM358-N D/S doesn't have output voltage swing spec when Vs=+5V as follows,…
Part Number: LM358A Hi Team,
Below is customer application circuit, they use LM358A and find some devices doesn't meet their production criteria .
NG 5PIN:2.8mV、7PIN:21.5mV
OK 5PIN:2.1mV、7PIN:15.5mV
The output voltage offset will cause customer circuit…
Part Number: LM358A Other Parts Discussed in Thread: TINA-TI , LM358 , LM358LV
Hi team,
I am using LM358A as a non-inverting amplifier to simulate the circuit. When the input signal is 10mV, the output waveform looks normal; when the input signal is 50mV…
Part Number: LM358A Other Parts Discussed in Thread: LM358
Hi Experts,
Good day! I am posting this on behalf of the customer.
My customer is using your LM358A in a capacity water tank level sensor. When I'm testing the RF common…
Part Number: LM358A Other Parts Discussed in Thread: LM358 , , TLV9062 , LMV358A , TLV9002 , LM7705 Hi,
We are using CC3220MODSF12MBR and LM358AIDR to read the analog voltage, working fine.
1. Now we have to measure the DC current using shunt resistor. My…