Part Number: LM833-N Other Parts Discussed in Thread: LM833 Hello,
Do we have the PSpice model for the LM833M available for a customer? I'm unable to find it.
Thanks,
Darren
Part Number: LM833 I had received the answer and now I have one more question
In this case, what is the excactly meaning of Q?
Resonance frequency or Quality Factor or another ? I'm a little bit confusing of meaning of Q
Please answer me.
======…
Part Number: LM833 Other Parts Discussed in Thread: OPA1602 , Oscillation question about inverting op-amp circuit(about LM833DGK).
The circuit is configured as shown in Appendix 1, with a oscillation of 0.54v for input(A) and 1.19v for output(B) (The oscillation…
Part Number: LM833 Hi,
We use LM833 to amplify the audio signal with VCC+/VCC- at +18/-18V.
On datasheet,±18V is the recommended operating condition,but also the maximum VCC is ±18V,like below.
So we are worry about our application,is LM833…
Part Number: LM833 Hi,
We use LM833 to design the mic pre-amp as 'Single-Supply, Electret Microphone Preamplifier Reference Design' recommended,then the audio input(called device1) transmit to another device(called device2) which is the same design.…
Part Number: LM833-N Other Parts Discussed in Thread: LM833 , LMP7732 , LME49721 Hi Team,
Could you help double check what's the min single power supply for LM833-N ?
Is it 5V ?
It's not quite clear in spec. My customer would like to use 3.3V for supply…
Part Number: LM833 Other Parts Discussed in Thread: LMC6482 , OPA1688 , OPA2134 Dear Engineers,
Can the LM833 be driven continuously into Ground saturation without phase reversal given that current is limited into its pins. I have a circuit where I need…
Part Number: LM833-N Other Parts Discussed in Thread: LM833
Hi,
I just built a x1000 low noise amplifier based on Fig.2 of "Design of ultra low noise amplifiers" by Vojtěch Janásek, using an LM833.
It works perfectly but the noise is…
Part Number: LM833 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Hi everybody I try to simulate this circuit with LM833 opamp in TINA tools and Webench But I received differrent results With input signal from +/-2V Output…