Part Number: LMH6518SQEVK
Hi,
I am using LMH6518 EVM to amplify the signal.
I am providing PAM3 signal as an input & measuring output of amplifier.
There is some eye opening at input side (eye height is 26mVpp) but output of amplifier gets noisy…
Part Number: LMH6518SQEVK Hi,
I am using LMH6518 EVM to amplify the signal.
In LMH6518 datasheet, it is mentioned that over-voltage clamp can be set using SPI but in SPI i can see only 1 register through which i can set only bandwidth, ladder attenuation…
Hi Wilson,
Yes the LMH6881 Eval module comes with the USB2ANY board / controller and necessary cables and software / GUI for download (http://www.ti.com/tool/lmh6881eval).
The LMH6518 EVM, however, is controlled with its own USB interface board (http…
Hi Ali,
The LMH6518 EVAL board is a 4 layer board (inner power and ground layers) with several vias to copper areas on the other 3 layers for good thermal conductivity. Does your test board have these provisions for good power dissipation? An indication…