Part Number: LMV611 Other Parts Discussed in Thread: LP2985 Dear Expert
① Test method: The oscilloscope uses Tektronix's TDS2024C. After the operational amplifier is powered on (the operational amplifier is powered by LDO output 3.0V, model LP2985), keep…
Part Number: LMV611 hi dear supporting team,
how about the CMVR of LMV611 at TA=95degree and TA=100degree? customer is using it as a comparator, Vin+=0.8mV, Vin- =8mV, the output should be low voltage, while at TA=95degree, they find the output will be…
Part Number: LMV611 I see the following parameters in the data manual of LMV611. I want to know how much CMVR is when the temperature is between 85~125℃. Is there any relevant test data and CMVR-temperature curve?
Part Number: LMV611 I see that the CMVR of LMV611 in the data manual is related to temperature. Will there be a long time drift in this CMVR? For example, the CMVR range of a LMV611 I used at 85℃ is just between V - and V +, which meets the data manual…
Part Number: LMV611 Customer is considering large load capacitance / voltage follower circuit of LM611.
※The reason of large CL is output side connecting many(36line) NAND Flash and SoC.
If there problem(unstable) for below circuit, please let me know…
Other Parts Discussed in Thread: LMV611 , TLV6001 TINA does not appear to have a model for the TLV6001 or the LMV611. Which part that is in TINA would be closest and best to use?
When will TINA have these parts added?
Other Parts Discussed in Thread: LMV611 Hi, with single supply 3,3V, as voltage follower, I wonder: (A) Is it guaranteed to be latch-up free up to some current? At least 10mA would be nice. Note: It can have this input current both when supplied with +3…
Part Number: LM321 Other Parts Discussed in Thread: LM7705 , OPA341 , TLV341 , LMV611 , TLV2211 Hello, I'm searching for an OPAmp same package and pinout as the LM321 but with more sink current (>5mA) at 0V Vout.
Regards, Holger