Other Parts Discussed in Thread: MSP-TS430PM64 , MSP430F4152 , MSP430F2234 , MSP430F2370 , MSP430F2350 , MSP430F2330 , MSP430F2274 , MSP430F2254
Hi,
We have a kit contents called MSP-FET430U64A which contained
one MSP-TS430PM64 target…
Other Parts Discussed in Thread: MSP430F2330 , MSP-TS430QFN23X0 Hi, All,
I use MSP430F2330.
And I made a catastrophe by erasing the information memory A, that amounts to 700 pcs.
1. Is there any tool to recover?
2. Is there any service regarding the…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
OK, got an .rl file. See attached.
The line in question in this file is line 42960, __bis_SR_register(GIE). If you look, it replaces that line with the following:
__asm__ __volatile__ ("bis.w %0, SR { nop" : : "ri"((unsigned int) (0x0008)) );…
V6MSP430.dll.txt V7MSP430.dll.txt Hello Jace,
The first file is V6 DLL and second file is V7 DLL. I had to add the .txt extension since uploader won't allow .dll
Dave
Hello Pavel,
EDIT: I didn't read past your first error. You already did this, and I didn't notice.
Pavel Hristov said:
We tried adding the following lines in io.h
#elif defined(__ MSP430F6726 __) #define __MSP430_6726__
For your first error, you…
Other Parts Discussed in Thread: CCSTUDIO I have been trying for the last week to install CCS 5.2 onto a new computer with no luck. It appears some of the features install but not all. I require assistance to the problem. Below is the log.
[ Edited by…