Part Number: MSP430F6769 Hi
TI has a list of MSP-TS430PZ100X sockes. But I reviewed them and no one is compatible with MSP430F6769 100 pin. Is there any socket to be used of this device?
best regards
Legend Chang
Part Number: MSP430F6769 Dear Champs,
I am asking this for our customer.
Is an external crystal required?
Without an external crystal, it seems DCO could not set internal oscillator freq. directly with FLLREF?
Would you please help clarify it?
Wa…
Part Number: MSP430F6769 I would like to know the input loading characteristics of the external voltage reference on the following 24-bit Sigma-delta ADC modules on MSP430:
SD24 on MSP430I20xx,
SD24_A on MSP430AFE2xx,
SD24_B on MSP430F67xx(A),
Specifically…
Hi MSP student,
I'm attaching a list of devices supported by SYS/BIOS (the RTOS):
3276.devices.html
If you want TI-RTOS, which includes SYS/BIOS as well as driver support (SPI, UART, etc), the list of MSP devices supported by TI-RTOS is the following…
So I just found something interesting! I have a PC with a clean install of win10, and I installed CCS 11.2 with the command line "--mode unattended --disable-components PF_MSP430,PF_MSP432"
And then installed the arm compiler and tried to use…
As one more update, you can find the full revision table of compatible hardware and software revisions included in the release notes:
Release-Notes-MSP-GANG.htm
See the section called "Version Matrix"
Hi SeaFesse, If you check the release notes from version 1.2.8.0, in the Version Matrix section, you'll see that the MSP-GANG HW v1.04 is only compatible with version 1.2.1.0 and higher. So this combination should not be used - please use the latest…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…