Hi Ashwani Goel,
I have reviewed the datasheets for the TMDS64EVM and TMDS243EVM. These evaluation boards do not meet our specifications (PROFIBUS, PROFINET, ETHERCAT), and the form factor of these cards is larger compared to the TMDSICE3359. Could you…
Part Number: AM3357 Other Parts Discussed in Thread: PROFIBUS , Hi, My customer released Profibus slave product using AM3357. One of their end customers reported a communication error happens periodically. According to their investigation, the error happens…
Part Number: DAC8742H Other Parts Discussed in Thread: PROFIBUS , Hi to all,
We are working with one customer who is interested in developing a device that could support all the three protocols the DAC8742H offers. This part fit perfectly in their requirements…
Part Number: THVD1450 Other Parts Discussed in Thread: SN65HVD1176 , PROFIBUS , Hello
Both SN65HVD1176 and THVD1450 datasheets says they support profibus.
Does it mean both devices comply IEC61158-2 Profibus standard and Profibus certification test specification…
On Linux:
We do not support Profibus.
Here is the list of Industrial protocols supported on Linux.
https://software-dl.ti.com/processor-sdk-linux/esd/AM335X/08_02_00_24/exports/docs/linux/Industrial_Protocols.html
On RTOS:
https://software-dl.ti.com…
Part Number: AM3356 Other Parts Discussed in Thread: PROFIBUS Hi
We are having an existing board with AM3356 which has the following interfaces
16 bit DDR3 RAM
8 bit NAND Flash
RGMII1 and RGMII 2 used for Gigabit ethernet
UART0,UART1,UART3 and 5 use…
Hi Shotaro-san,
Thanks for following up with additional question.
Please note that the currents specified in supply current characteristics tables are based of actual characterization measurement data. The typical and maximum currents observed are also…
Part Number: PROCESSOR-SDK-AM64X Other Parts Discussed in Thread: PROFIBUS Hello everyone,
After being busy with other things for a long while, this week I have been looking at the Sitara AM64x family and I've noticed the datasheet refers to Profibus…
Part Number: TMDSICE3359 Other Parts Discussed in Thread: PROFIBUS
Fast traslate
Icon translate
Hello,
I have installed the Profibus_Slave sample software and I can update the software with the SD card. I looked at the Profibus_Slave…