Part Number: SN74LVC1G79-Q1 Hi experts,
These parts have MSL level marked as NC, while the same part# of another DC has the detailed information.
These were from TI Franchise. Datasheet shows that the MSL of this item is Level 2.
What's the meaning of…
Part Number: SN74LVC1G79 Other Parts Discussed in Thread: SN74HCS74 Does this part (likewise, the "LVC1G80, 'LVC2G79 and 'LVC2G80) have any type of internal power-on reset that guarantees the start-up state of the Q (or /Q) output? Or do they just…
Part Number: SN74LVC1G80 Other Parts Discussed in Thread: SN74LVC1G79 , , SN74HCS74 My customer want to default output low level,but when use SN74LVC1G80,it default output low level.Can I use SN74LVC1G79 to output low level by default?
Blow is the customer's…
Part Number: TCA9543A Other Parts Discussed in Thread: TCA9546A , SN74LVC2G66 , SN74HCS74 , SN74LVC1G79 , SN74LVC1G175 Hi,
I would like to know if this is possible:
I think it is wrong because there is an address conflict, all TCA9543A have the same address…
Part Number: SN74LVC1G79-Q1 Hi Team
What does the ΔICC represent in the datasheet?
What's the difference with ICC?
How should ΔICC be applied when calculating the total current consumption of an IC?
Thank you
Part Number: SN74LVC1G79 Please let us know if the Part Number SN74LVC1G79DBVTE4 is Active/Obsolete/Invalid.
If Active, provide us the YTEOL(Years to End of Life Information).
If Obsolete, provide us the supporting documents i.e, EOL notice, PCN along…
Part Number: SN74LVC1G79 Hi Expert
When using SN74LVC1G79 (VCC is 5V, D is pulled up to 5V via a resistor), during power up, before CLK high logic come, the output already output high.
To check more, Pin D and Pin CLK are both floated, then it is found…
Part Number: SN74LVC1G79 Other Parts Discussed in Thread: SN74HCT574 Hello Sir/TI,
Currently, we are using SN74LVC1G79. I would just like to ask if TI has data on VOH typical values. The datasheet only shows minimum values like as shown in screenshot below…
Part Number: SN74LVC1G175 Other Parts Discussed in Thread: SN74LVC1G374 , SN74LVC1G79 , SN74LVC1G80 Hi team,
Are below devices able to work as frequency divider (Fclk -> 1/2Fclk)
>SN74LVC1G175
>SN74LVC1G374
>SN74LVC1G79
>SN74LVC1G80
Best…
Hello,
Unfortunately we do not have any characterization data for the jitter level of this device.
Please note that we are trying to ensure that all posts are answered. With any new posts, we will be sure answer in a timely manner so that no posts…