Part Number: TCAN332EVM Other Parts Discussed in Thread: TCAN334 , We are considering using TCAN334. The circuit diagram of TCAN332EVM is used as a reference.
question 1: Are there any recommended products for L1 and D2? Please tell me the manufacturer…
Part Number: TCAN332EVM Other Parts Discussed in Thread: TCAN332 , SN65HVD1050 Hi,team.
I want to operate TCAN332EVM with split termination and nomal mode. i have 3 question.
①How should I set JMP 6?
②I think , I can operate split temination mode with…
Part Number: TCAN330 Other Parts Discussed in Thread: TCAN332EVM Hi.
A question about the Test Points in CANH & CANL in TCAN330 EVM board.
The board has TPs directly connected to the CAN signals and other TPs connected to the signals through a resistor…
Part Number: AM625 Other Parts Discussed in Thread: SK-AM62 , TCAN332EVM , TCAN332 Hello,
I connected the SK-AM62 board to a TCAN332EVM board.
The PIN CAN_RX/TX (8/10) from the user expansion connector are connected to RX/TX pin of the TCAN332EVM board. …
Nenad,
You used the phrase “full functionality” for CAN. The ControlCARD+Docking station eco-system does not have CAN transceivers. Sure, you can run the loopback test. However, for you get the “true feel” of the CAN bus, you need to run some tests that…
Hi Carlo,
Sorry, we don't have a C2000 EVM that has more than one CAN transceiver. I can think of a couple options you could try below:
Wire CAN signals (and Ground) to a 2nd C2000 LaunchPad CAN transceiver pins. LAUNCHXL-F280049C would probably…
Hi Harrison,
There is a reference schematic in the EVM User's Guide. You can find it here:
www.ti.com/.../sllu231.pdf
The folder for the EVM board is here:
www.ti.com/.../tcan332evm
Let me know if you need anything else.
Best regards,
Max