Part Number: TIDM-1PHMTR-ESD Other Parts Discussed in Thread: MSPM0G3507 Hi team,
My customer would like to design e-meter and there is reference design in EERD.
TIDA-010036 reference design | TI.com
But I think those TI components are little old for deign…
Part Number: TIDM-3PHMTR-TAMP-ESD Tool/software: According to refrence circuit diagram of TIDM-3PHMTR-TAMP-ESD, two 4148 diode were used at each AVCC and AGND line (I+, I-)
I found that someone also asked same question and TI e ngineer replied like below…
Part Number: TIDM-3PHMTR-TAMP-ESD Hello Team,
To protect ADC pins of MCU, clamping diodes are essential. If the input voltage of an ADC pins is maximum of let us say, 3.6V, the clamping diode of 0.2V to 0.3V should be used when the diode is connected…
Part Number: EVM430-F6736 Other Parts Discussed in Thread: TIDM-1PHMTR-ESD Tool/software: Code Composer Studio I'm not able to find the latest source code that is running in EVM430-F6736 rev A .
I compared the hex files of SLAA517 and TIDM-1PHMTR-ESD…
Part Number: TIDM-1PHMTR-ESD Other Parts Discussed in Thread: TIDM-3PHMTR-TAMP-ESD , , TVS0500 , MSP430F67791A
Hello,
with regard to the emi filter at both voltage and current front end, if I rightly understood, this is only a differential mode filter …
Part Number: TIDM-1PHMTR-ESD Other Parts Discussed in Thread: MSP-EM-DESIGN-CENTER , , MSP430F6736 , MSP430F6736A , EVM430-F6736
Tool/software: Code Composer Studio
Hello,
I am trying to port code from IAR to CCS.
I am getting error of unresolved symbol…
Other Parts Discussed in Thread: MSP430F6736 , TIDM-1PHMTR-ESD Dear TI
I have read the slaa517e,which is a doucument of Implementation of a Single-Phase Electronic Watt-Hour Meter Using the MSP430F6736(A) , in breif called TIDM-1PHMTR-ESD.
I have a question about the…
Hey Naveen,
What is the line voltage amplitude and frequency? What is the minimum signal bandwidth required? Are you set on a certain microcontroller and just need sensors?
If you need isolation sensors, then you can examine the following products below…
Part Number: TIDM-1PHMTR-ESD Hi anyone
This may be a basic question...but...
In the design for the TIDM-1PHMTR the power to the board is from supply live and supply neutral to an R-C voltage reducing and rectifying circuit ending at an TPS77001.
Supply…
Part Number: MSP430F6779A Other Parts Discussed in Thread: TIDM-3PHMTR-TAMP-ESD , MSP430F6779 Tool/software: According to refrence circuit diagram of TIDM-3PHMTR-TAMP-ESD, two 4148 diode were used at each AVCC and AGND line (I+, I-)
I found that someone…