Part Number: DAC5311-Q1 Other Parts Discussed in Thread: TIPD153 , DAC5311 Dears,
VOUT output passes through the wire harness to another controller. What protection circuit should be added to the VOUT pin? Used in tractor cars, the environment is more complex…
Yulei,
What is the DAC8760 hardware platform that this test is being conducted on? An EVM board? An EMC-EVM board? Custom hardware? If it's custom hardware, can you share the schematic? RF artifacts may not entirely be dependent on devices soldered to…
Part Number: DAC8760 Other Parts Discussed in Thread: TIPD153 Dear Specialists,
My customer is considering DAC8760 and has questions.
I would be grateful if you could advise.
---
(1) How is the configuration HART-IN pin if HART is not used.
Should it…
Other Parts Discussed in Thread: DAC7760 , DAC7750 , XTR110 , XTR111 , XTR300 , TIPD153 Hello,
In our application, we required constant current source IC which can give output current between 0 - 20mA.
Also if I wish to design a circuit for the same above application…
Duke-san,
Thank you very much for your prompt reply and detailed explanations.
Your answer is very helpful to me.
Please let me ask you an additional question.
According to TIPD153, I think that it would be better to connect the C1 capacitor between…
Hi Shinichi,
Thank you for your query. For question 1, if you could ask a more specific question I can check with the design team and get back. We will not be able to share the design level architecture. For question 2, you can refer to the following…
Hello,
It sounds like you're familiar with at least one of the TI Designs related to the DAC8760 - there are several floating around ti.com from various groups within TI. The TI Design (tidu392.pdf) you mentioned uses one approach to deliver IEC61000…
Hi John,
Take a look at the DAC8760, or a DAC + XTR combination like the design shown in TIPD155 .
We also have a few reference designs featuring the DAC8760. Take a look at TIPD119 and TIPD153 .
Hello,
I've provided answers to your questions below:
Clamp diode to protect A1 from -.5V at pin 4: -consider the BAT54 Schottkey diode.
A suitable external mosfet that is not in a to-92 package (I can not find this from available recommended parts…