Part Number: TLV3502-Q1 Other Parts Discussed in Thread: TLV7034 , TLV3502 , LMV331-N Hello:
The customer designed two peak sampling circuits using TLV7034 and TLV3502 respectively, with the same parameters. However, when using TLV7034, it was found that…
Part Number: TLV3502 Other Parts Discussed in Thread: TLV3501 , TLV3604 TLV3502 seems to have very low input bias and offset current in pA at low propogation delay at 4.5ns.I presume that the input pin is connected to CMOS. LT1720 from linear technology…
Other Parts Discussed in Thread: TLV3502 , TLV3501 Hi ,
Can TI provide TLV3502 PSpice model ?
I need TLV3502.dsn and TLV3502.lib files to do PSpice simulation.
thx
Best Regards,
Arang
Part Number: TLV3502 Hello,
I just want to confirm that these two devices (TLV3502 & TLV3502-Q1) are the same silicon, the Q1 just has additional testing for the automotive qualification.
Thanks,
Nick
Part Number: TLV3502 Hi,
Good Day. My customer is considering using TLV3502 in a new design, and he found the specified input offset voltage max is +/-6.5mV, while the specified overdrive voltage can be 5mV(less than 6.5mV). Seems these two parameter is…
Hi All,
Increasing the resistance value and keeping the hysteresis 50mV has proven to remove the glitch or delay we are seeing above. One more point the testpoint wires added to the problem which has also been resolved now.
Thanks.
Part Number: TLV3502 Other Parts Discussed in Thread: , TLV3501 Dear sir,
Good evening.
Kindly provide us TLV3502/TLV3502-Q1 spice model to simulate in TI for pspice.
We found only TLV3501 spice model which has shutdown feature in TLV3502 product reference…
Part Number: TLV3502 Hi ,
We are using TLV3502AIDCNR part in one of our design. Could you please help us how to decode this different bottom marking.
Thanks
Part Number: TLV3502 Other Parts Discussed in Thread: TLV3201 , Is there an evaluation board for TLV3502 and TLV3201? I don't see one on the product folder page. If not, is there a coupon board?