Part Number: TLV3704 Hello,
We want a hysteresis comparator with low current consumption for an automotive battery-voltage sense application with 3.0 ON and 7.9V ON switching points.
Our built-up circuit (se below) given a goog values, but the calculation…
Part Number: TLV1702 Other Parts Discussed in Thread: TLV7042 , TLV7032 , , TLV1704 , TLC3704 , TLV3704 Hello
We are considering to use TLV1720.
In our circuit, the output of TLV1720 must be high impedance.at low voltage below 2.0V.
Does TLV1720 behave like…
Part Number: TLC3704 Other Parts Discussed in Thread: TLV3704 , TLV3494 , LF411 I'm looking for some technical rationale for the common-mode voltage limit of Vcc-1.5V.
I have a legacy design that breaks this rule, but has worked just fine. (Vcc =3.3V…
Part Number: TLV3701-Q1 Other Parts Discussed in Thread: TLV3701 , TLV3702 , TLV3704 Hi team
TI.com shows same FIT = 0.4 for TLV3701(1 Ch)/TLV3702(2 CH)/TLV3704(4 Ch) comparators.
I think the FIT calculated by TI.com is based on 1 Channel.
user has to sum…
Hi Lis
May I get your swift response again ?
thanks a lot.
[Q1] you means like below ?
the FIT calculation on TI.com is based on 1 channel,
so that OPA348(1 Ch)/OPA2348(2 Ch)/OPA4348(4 Ch) should have same FIT = 1.6,
however, if customer uses OPA348…
Part Number: LM339-N Other Parts Discussed in Thread: LM339 , TLV3704 Hi,
My customer is using LM339-N. He has questions about input voltage range.
Condition is V+ = 5V and V- = GND. Q1: Can we use LM339-N with INPUT+ = +1V~+9V(swing signal) and INPUT- …
Hi Vindhyachal,
I work with the TLV3701, TLV3702 and TLV3704 a lot, and sometimes forget which one I am dealing with when typing. Indeed, I meant the TLV3701 for your application.
The TLV3701 meets all of the application needs and would be the choice. …
Other Parts Discussed in Thread: TLV3401 , TLV3404 , TLV3704 , TLV3701 Hi
I am using TLV3401 to get the output of the Motion Sensor and Sound/Clap sensor as attached.I am giving 3.3 volt to the opamp and the comaprator.
Now Problem when i connect the R32…