Part Number: TLV4112 Other Parts Discussed in Thread: TINA-TI , LM7332 Hi,
I'm interested in using the TLV4112 amplifier (for its high output current) in a Sallen Key low pass filter unity gain configuration. The cutoff frequency is 1kHz.
The op-amp…
Part Number: OPA569 Other Parts Discussed in Thread: TLV4112 , OPA567 Tool/software: Dear Sir,
OPA569 is too bigger , can you suggest a similar type with small size and small current (0.3-0.5A)?
Best regards!
David
Part Number: TLV4112 Other Parts Discussed in Thread: TLV2772 , TLV4111 , , TINA-TI , LM7332 , UA741 Purchased 2 of these TLV4112CP for a new design because the TLV2772CP could not drive my load. MY design worked fine with the TLV2772 as long as the load was…
Part Number: TLV4112
Hi, op-amp experts:
We need to use the op-amp to make sure VIO_IN<VCCA as showing by circuit below; MCUVCC=3.3V, VCCA range is from 2.8V to 5.5V. What's about VCCA<3.3V which makes the op-amp VIN > VCCA? is there a input protection…
Part Number: TLV4112 This could be me struggling with reading the datasheets, but I couldn't find the ratings for this amplifier.
I want to power this amplifier with +/-5V power supply. In page 3 (absolute maximum ratings), the differential input…
Part Number: TLV4112 Other Parts Discussed in Thread: LMC6482 I am trying to use LTV4112 as a dual op-amp circuit to interface with an electrochemical sensor.
The operation depends on having high output current (max 360mA) but low input bias current. …
Part Number: TLV4112 Other Parts Discussed in Thread: TLV1171 , LM2991 , TPS795 I am not sure if this is a simple question (I am not very experienced with electronics).
I want to use the TLV4112 op amp in a circuit where it is going to pass high current…
Other Parts Discussed in Thread: TLV4112 hello,
I am going to drive TLV4112 by TPS780300250DRV, set to 2.5V output.
will TLV4112 work safe at 2.5V power supply, does it need any margin at the low side of the specification.
thanks,
David Sun