Part Number: TPA3255EVM Other Parts Discussed in Thread: TPA3255 , I am working on a project where we are interested in using the TPA3255 to power a magneto strictive actuator. This actuator requires higher voltage than the TPA3255 can provide (81VRMS)…
Part Number: TPA3255EVM Other Parts Discussed in Thread: TPA3255 , , TPA3245 Hello
i'm using the TPA3255 AMP, and i would like to implement the TPA325x Post-Filter Feedback to it as described in the (SLAA788A - Application Report)
now as i see in the …
Hello Muhammed, I would only recommend using Q1 if you are using it for automotive applications, functionally the devices would be the same.
best regards, luis
Part Number: TPA3255EVM Other Parts Discussed in Thread: TPA3255 , Hello team,
We are presently incorporating the TPA3255 Class D IC into our design.
Could you kindly provide us with the Gerber files for the TPA3255EVM as a point of reference?
Thank yo…
Part Number: TPA3255EVM Other Parts Discussed in Thread: TPA3255
Hello Team,
Could you kindly explain the technical distinctions between the TPA3255EVM and TPA3255D2EVM?
Regards
Pavan P
Part Number: TPA3255EVM Other Parts Discussed in Thread: TPA3255 We are trying to drive Shaker with the TPA3255EVM board.
We tried to BTL output configuration. We measured 5.6 A at the output and 75 g at the Shaker.
We tried to PBTL output configuration…
Part Number: TPA3255EVM What mates with J28 / J30 (Audio Interface Board) on the TPA3255EVM?
and, BTW, the BOM is INCORRECT concerning the Part Number for J28.
BOM says it is a Samtec SSQ-108-02-G-D. That would be a 8x2 connector.
The actual part on the…
Part Number: TPA3255EVM Other Parts Discussed in Thread: TPA3255
Hi, guys
Sorry to bother, I have searched some of the posts about using speaker amplifier beyond audio application, but I can't find solutions to mine.
My application is to drive inductive…
Part Number: TPA3255EVM Hello everyone,
I make some tests in TPA3255EVM, in PBTL mode. I wanna make 600W for output power, fot that i connect power supply 53Vdc, and 21A, and, the load is a resistor with 1.9R. Input is a senoidal signal with 3.3Vpp and…