Part Number: TPS561201 Again, the TPS561201 doesn't exist in Webench. Second time now I've tried, DIRECTLY this time from the TI website as instructed by Shipeng Cheng from the support forums instead from the data sheet downloaded from Digi-Key…
Part Number: TPS561201 webench does not recognize this part. Every time I enter it Webench shows designs for a totally different part number(s). When will Webench be updated to recognize the TPS561201?
Part Number: TPS561201 Hi team,
My customer want to check if aluminum electrolyric capacitor can be used for both Cin and Cout. It seems that ceramic capacitor are recomended in the datasheet.
Regards,
Ohashi
Part Number: TPS561201 I plan to use TPS561201 to input 5V and output 2.5V, but the usable area on the PCB is only about 9mm * 19mm, so I can't design a pattern with as much margin as the evaluation board (TPS561201EVM-896). Please provide a better…
Part Number: TPS561201 Hello team,
My customer has 2 questions. Can you tell me your opinion?
Can we apply 5.5 V and 17 V to VFB and SW with Vin=0V condition?
If possible, do we have any additional circuit into VFB and SW? Competitor device has recommended…
Hi
Your average current is just 0.6A. When inductor current from 1.7A to 1.2A, OCL protection will be triggered, LSFET will have the highest priority to turn on.
One current be lower than 1.2A, protection logic will be canceled. The turn on/off behavior…
Part Number: TPS561201 Other Parts Discussed in Thread: TPS563201 Hi team,
Customer changes buck converter to TPS561201 from TPS563201 due to current limit. Is it able to reuse all passive components? Are there recommnedation of the replacement?
Regards…
Part Number: TPS561201 Hi Team,
Whether TPS56120 can achieve customer requirement as below?
5V input
-2.5V output
100mA load
The schematic is attached, could you please also help review it, thanks for your help in advance.
BRs,
Francis
Part Number: TPS561201 Hello guys,
One of my customers has the following question about TPS561201 OVP threshold voltage.
Q. What is the OVP threshold voltage?
The customer couldn't find the voltage in the device datasheet. Your reply would be much appreciated…
Part Number: TPS561201
Hi All,
We considered TPS561201 part in our design.
We would like to check on similar pin mapping switching regulator availability which accepts 2.7V input range?
Current rating from 500mA to 1A is acceptable.
Please suggest any…