Sounds good. I am going to mark this thread as resolved, but feel free to reopen it if you run into issues related to this thread.
Kind regards,
Conner Gillette
Shane,
What EVM should I buy:
TUSB320EVM
TUSB320-HA-EVM
TUSB320-LA-EVM
What is the difference?
Is there another eval board needed? Like the HD3SS2522?
I think the HD3SS25ss is obsolete?
Part Number: TUSB320LAI Other Parts Discussed in Thread: TUSB320 , TUSB320-LA-EVM I need to charge a Li-Ion battery with max 1.5A over a USB-C plug. I want to use a TUSB320 to determine the max. current I can draw from the power source. If the power source…
Part Number: TUSB320-HA-EVM Other Parts Discussed in Thread: USB2ANY Hi TI expert
I would like to know if I can use USB2ANY to configure a TUSB320-HA-EVM board.
Best regards,
Thomas
Part Number: TUSB320-LA-EVM Other Parts Discussed in Thread: TUSB320EVM , TUSB320 Hi team
Regards to TUSB320LA-EVM, I have below problems need your help to clarify. Thanks!
As TUSB320 datasheet mentioned below, UFP mode can support Accessory mode with…
Part Number: TUSB320 Hello: I am a new E.E. quite new to touch Type-C USB design, what I try to do is first to have EVM of TUSB320 to figure it out. But I have found that there are TUSB320-EVM, TUSB320-LA-EVM and TUSB320-HA-EVM. I am confused that what…
Part Number: TUSB320EVM Other Parts Discussed in Thread: TUSB320 Dear Sir,
May I know, if TUSB320 EVM can work in DFP mode with 5V adaptor attached then output 3A from typeC port?
My customer did some testing with EVM but still fail to get 3A from typeC…
Hi,
Thanks for the response.
Please see the attached GUI plot of ECG 1 and ECG 2 showing a difference in amplitude
The test signals were taken from an ECG simulator, with the following connections to the AFE EVM board:
LA to EX1 RA to EX2 LL to EX3 RL to…
Part Number: LP-MSPM0C1104 Other Parts Discussed in Thread: MSPM0C1104 , Tool/software: Hi experts,
I am developing UART function based on the example "uart_echo_interrupts_standby_LP_MSPM0C1104_nortos_ticlang'
I found that if I configure the…