Part Number: EV2300-084 Other Parts Discussed in Thread: TUSB3410 , TUSB6250 Tool/software: I’m trying to get the EV2300 working on Windows 11 (64-bit). I have a modified version of the driver’s INF file that attempts to enable compatibility with Windows…
Hello Paul,
the EVM is not designed for self-sufficient operation. The user guide of the EVM ( www.ti.com/.../scau025) contains the schematic.
The TUSB3210 microcontroller is directly connected to the CDCE18005. The microcontroller 3.3V supply is derived…
Part Number: TUSB3410 Got this error message:
There was an error trying to install the driver for the device, you will need to install it manually.
Trying manually install <TUSB3410_Apploader.inf> from <C:\Program Files (x86)\Texas Instruments Inc…
Other Parts Discussed in Thread: TAS5086
Hello
My customer had bought New TAS5132DDV2EVM( TAS5086 ) , but customer and I
can not have USB connection , ( no ping/pong sound when USB insert to PC, LED3 of HPL-MC012 is
distinguish, usb driver searching…
Good point. It looks like the VIN threshold is 2V for the TUSB3210. So, this looks to maybe be a problem.
I will probably just add the level shifter to the cable from EV2300 as you suggested.
Just to confirm, it is the SMBUS connection of EV2300…
Hi Mohammad,
The 0x0451 VID is the Texas Instruments Vendor ID, so if any other TI devices are connected to your USB ports they may also show up with the 0x0451 VID.
Based on www.ti.com/.../slla154.pdf , assuming that the 0x2136 PID is a power-on…
Hello Brett,
I'm glad the GPIB-to-USB interface worked for you!
1) The pre-cal and post-cal file paths are controlled by the model file. In the "Configure Cal" tab, you can create and edit pre-cal and post-cal files which can then be loaded into a…
Hi!Bolurian:
well! In fact, I found the real problem! This is USB-TO-GPIO EEPROM (24LC64) The program inside has been deleted! I found a lot of similar situations using Google search and TI E2E search. Now I have two solutions: method 1. Using an EEPROM…