Part Number: PRU-ICSS-INDUSTRIAL-SW Other Parts Discussed in Thread: AM3357 In our implementation we leverage a single port (Port 0) of the RMII interface and MDIO of the AM3357 to communicate via EtherCAT through the PRU-ICSS and a DP83826 PHY. To do so…
Hi,
I do not have any new update here. From previous discussions I see there was some inconsistency in PHY register values between the working and non-working case. For this I had asked to check for the 4 points mentioned in my previous 2 replies. If there…
Part Number: PRU-ICSS-INDUSTRIAL-SW The wiki state that one of the known limitation of the HSR/PRP module is the following:
PINDSW-4227
Sitara
A few packets are truncated during forwarding if continuous burst of packets are send to DUT at line rat…
Part Number: PRU-ICSS-INDUSTRIAL-SW Thank you for your hard work.
I have a question.
I understand that pru-icss supports IEEE1588. Exactly, supporting 1588v2? Or, are you supporting 1588v1? Or are they both compatible?
If you have a reference document,…
I am not able to get the SW UART to work on the Beaglebone black and I am not sure what I am issing.
Board: Beaglebone black
Base Image : am335x-debian-11.7-iot-armhf-2023-09-02-4gb
I have successfully compiled and installed a new kernel, with the options…
Hi, Yes, I think we should keep this track alive because I wanna be sure that the build process is done correctly. For thread: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1263030/pru-icss-industrial-sw-prp-bug-fix-issue/480…
Hello Ryan
Looks like we missed addressing this thread
I talked to the developers on this and got the following feedback
ICSSM in AM3/4/5 has some gaps due to inter packet gap (IPG) maintenance not supported in HW at 10Mbps. Any work arounds require…
Part Number: PRU-ICSS-INDUSTRIAL-SW I'd like to ask you two questions.
1. I understand that PRU-ICSS or PRU-ICSSG firmware and development costs are free, is it free even for commercial use? 2. I understand that PRU-ICSS does not support CIP-Sync.…
Hi Xiangju,
Apologies for the delayed response, I was not available the last week.
The dev team has reviewed the issue and they have suggested a working configuration for your use case - Utilising MAC port 2 and PRU GPIOs
Please follow the steps below…