This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VCA2612: How to input the differential signal to this chip

Part Number: VCA2612
Other Parts Discussed in Thread: THS4551

Hi all

When i use the VCA2612 for my IF amplifier , i can not find the details for the differential signal input

But the datasheet write that it support the differential signal input

So could you help me to check the schematic just as below and give me some advise . Thanks a lot

1、My IF signal is 1000ohm internal resistance output

2、The frequency of my IF signal is from 1KHz~20MHz 

3、i want to amplify the IF signal may be 40dB and then send it into ADC.