Part Number: INA210
Hello TI experts,
My customer now consider INA21[x} op amp for their new product, here is two types of schematic.
- PWM_CTRL is the PWM signal which low voltage is 0, high voltage is 1, frequency is 20KHz.
- when Q1 is on, the current of VDD_5V line is 2.5A (when PWM duty is 50%), and maximum 3A about 2 seconds.
- L400 is the coil which resistance is variable from the heat.
- in case2, the lower INA21x have 3V reference voltage. they designed it because they want more gain although they got little voltage difference compared to 5V reference voltage.
anyway my customer wants they have to get more effective output from INA21x even the voltage difference is little.
what do you think that which one is proper, case1 or case2?
please let me know if you need more information to review these schematic. Thanks.
Best regards,
Chase