This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VCA2612: Where do i have to place the capacitor for compensation when using active feedback

Part Number: VCA2612

Hello,

in a hardware design i am using the VCA2612 with two differential input signals. The VCA2612 provides a compensation when using active Feedback. The value for the capacitor is calculated with Equation 4 in the datasheet (see below).

The Question for me is where i have to place it for both channels (A and B)?

Is it between pin 10 (COMP1A) and 11 (COMP2A) for channel A and between pin 27 (COMP1B) and pin 26 (COMP2B) for channel B?

Or should I use Figure 4 as a guide and place the capacitor between pin 11 (COMP2A) and pin 16 (LNP_IN_PA) for the positive input and between pin 10 (COMP1A) and pin 12 (LNP_IN_NA) for the negative input of channel A?

In this case there is to place the capacitor for Channel B between pin 26 (COMP2B) and pin 21 (LNP_IN_PB) for the positve input and between pin 27 (COMP1B) and pin 25 (LNB_IN_NB) for the negative input, right?

Thank you in advance.