Other Parts Discussed in Thread: OPA521
Hello Texas Instruments team,
Please, when using TLV4111 as a volage follower, can i connect the Vdd pin to the input pin of the op amp ?
I have this question because this component is only rail-to-rail at the output.
If this doesn't work, is there an operational amplifier that can provide a similar current, is rail-to-rail input/output and could be used as a voltage follower with a 5V source ?
My application is :
I want to supply 5 V to different loads that are switched in the milisecond range.
The current provided to this impedances variates from 100 mA to 150 mA and they are not always activated.
My problem is that this impedance switch causes a variational voltage drop on my 5V line.
To solve this problem I thought about using an operational amplifier working as a voltage follower between the 5V and the impedances variation.
Best regards,
Rafael