This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV4021: I have a question about your PN TLV40x1 Specifically, TLV4041R5

Part Number: TLV4021


Hi,

Good Day. I have a customer who has a query with TLV40x1 datasheet. Please see below his concern for your reference. Thank you very much.

From the datasheet, table 1, the TLV4041R5 is specified as non inverting, with internal 0.5 V reference, push pull output

If I look on the figure in the same page, the TLV4041R5 is non inverting, push pull, but the reference is 1.2V

I believe this is an error just in the figure, I would like confirmation of this.

so the table 1 is correct, but the figures are not accurate, and I can refer to the table

yes, table 1 and table 2 are consistent is just the figure that is different

Best Regards,

Ray Vincent