Part Number: INA381
Hi,
I am using the IN381 as a overcurrent protection.
As you can see, i am using PWM to control the intensity of the LEDs. Thus the question i would like to ask is that if at 100% PWM duty cycle, the INA381 detect a overload, but when i change the duty cycle to 50%, will the INA381 still detect overload at the high level of the PWM?
If yes, are you able to advices how can i resolve this.. or should i change another detection method?