Other Parts Discussed in Thread: , OPA379
Hi,
I'm trying to simulate the OPA2333 op-amp and I used the OPA2333P model from https://www.ti.com/lit/zip/sbom166 since I couldn't find the OPA2333 model. The issue I’m having is that the OPA2333P model isn’t behaving as expected (please see below).
Using the OPA2333P model the current flowing in the op-amps’ input terminals is very high at 32mA! It should be close to 0A (i.e. pAs or nAs). Can anyone help explain this behaviour?
I tried a different op-amp (OPA379) and the current flowing in the op-amps’ input terminals is negligible (pA) as expected.
Regards,
Yemi