This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi There,
As the part:OPA2376QDGKRQ1 VSSOP is out of stock, any suggestion for footprint compatible alternative part to replace?
Thanks and Best Regards
Dong
Hi Dong
There are 2 possible options: The LMV842-Q1 or TLV2197-Q1. Note that the TLV2197-Q1 operates from 4.5 to 12V while the LMV842-Q1 goes from 2.7 to 12V