Part Number: OPA564
Hi,
I want to use the OPA564 with a single supply (0->12V) in order to amplify a sinus signal from a DDS to feed a coil.
If I understood the principle of the back-EMF problem, I believe that, because my supply voltage is +12V, a back-EMF can only be negative. If this consideration is true, do I need the diodes S1 and Z1 and S2 (figure 55 of the datasheet of the OPA564)? I believe I only need the Z2 zener diode with a low zener voltage (as low as 0.4V in order to be sure that the voltage at the output of the OPA never goes below GND-0.4V)?
In this case, if the voltage generated by the back-EMF goes below the 0V, the zener diodes becomes conducting and the current can flow through it.
Am I right?
Thank you!