Other Parts Discussed in Thread: TLV3704
Hi Team,
Customer is using comparator TLC3704 in one of the design, please see below query from component point of view:
- TLC3704 is powered up by using +/-3.3V. And As per datasheet, V.ICR is 0V to VDD-1.5 (for −40°C to 85°C) which makes the input voltage range -3.3V to +1.8V. Is this understanding correct?
- What is the impact on output or overall functionality of comparator if the input voltage violates above condition on any of the input pins (inv or non-inv)?
- Can you suggest alternate comparator parts (push-pull output stage with wide input range)?
Regards,
Naveen