Other Parts Discussed in Thread: THS3217,
I ordered two THS3217 EVMs to prototype a DC-coupled DAC driver circuit for a Xilinx RFSoC driving an I/Q mixer. I would like to connect +VCC to 6V and -VCC to -6V. However, it appears that -VCC is shorted to GND on both of the boards. I discovered this issue after the -6V rail of the lab supply immediately went into overcurrent mode upon power-up.
The manual does not seem to indicate that this should be the case. Do any components on the eval board need to be modified from the factory configuration?