Other Parts Discussed in Thread: INA190, INA240, INA228, INA229
Hello, I have been following with your colleague, and he redirected me to follow with you, kindly check the attached link, I'm looking for a current sensing amplifier, maybe you can redirect me to the correct option, I think I need a high-side sensing option, I have 6 batteries (1.2V each) for every 3 cells connected in series, another cell also connected in the same way, and by the end, I have a parallel connection which will feed the product with power(4.6-5V). The maximum current for this product could reach 900mA and the minimum 50mA. So will connect the shunt resistor and diode in series with the first 3 cells which are connected in series and check the current at this point through using the prober amplifier. The same thing for the other 3 cells, the same when the 2 series rails are connected in parallels, so I think I will need 3 amplifiers. Do you have any recommended amplifier for this scenario?
(+) BQ35100: BQ35100 - Power management forum - Power management - TI E2E support forums