This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1302: Is it safe to use AMC1302 in a 1500V inverter system?

Part Number: AMC1302

Dear TI,

I am going to buid an inverter prototype with 1500V DC-link voltage. The output voltage is 690V (L-L rms). I am wondering if AMC1302 can be used to measure the current or voltage in this situation? I see in the datasheet that the maximum isolation working voltage is only 1500V rms or 2121 peak DC. 

Any suggestion for this issue?

Thanks~