Other Parts Discussed in Thread: INA118
I have created an EMG Electrode circuit but I am having trouble with the 50Hz coupled noise from myself which is rather larger than I thought. Also the 50Hz has larger harmonics as shown below.
The signal to noise ratio has more noise than signal.
The Analogue Front End (AFE) passive components have been chosen to increase CMRR but I believe that it is not enough.
Resistors, 0.1% Tolerance
Capacitors, 1% tolerance
The circuit below has a notch filter giving good centre frequency of 50.1Hz and good attenuation.
However, I am still getting quite large harmonics.
Has anyone has similar issues like this?
Regards